Technical FAQs

Ask a Question

What are the replacement Diaphragms for Robert Shaw V3002-454-07 and V3025-3002 actuators

Issue:
What are the replacement Diaphragms for Robert Shaw V3002-454-07 and V3025-3002 actuators

Product Line:
Field Devices

Environment:
Maintenance

Cause:
Replacement 

Resolution:
Neither Robert Shaw actuators are available and the actuators have been obsoleted 30 yrs., with no replacement parts available.
REPLACEMENT:
For  V3002-454-07 valve/actuator assy a new MK-8811 actuator, with AV-496 linkage and VB-9313-0-5-14 valve body can be used , or assembly VK4-9313-802-5-14
For  V3025-3002 valve/actuator assy a new MK-6811 actuator, with AV-495 linkage and VB-9313-0-5-12 valve body can be used, or assembly VK4-9313-602-5-12
Was this helpful?
What can we do to improve the information ?