Technical FAQs

Ask a Question

Will a P1200AWK Circuit Breaker Enclosure Accept a Four Pole Circuit Breaker?

Issue:
Will a P1200AWK Circuit Breaker Enclosure Accept a Four Pole Circuit Breaker?

Product Line:
Molded Case Circuit Breaker Enclosures

Environment:
Installation

Cause
Selection

Resolution:
No, the P1200AWK is not UL tested or listed for use with 4 pole circuit breakers so they cannot be used in the enclosure. 

 
Was this helpful?
What can we do to improve the information ?