Technical FAQs

Ask a Question

What is the NEMA Rating for the 9999SC2 and 9999SC8 Hand-Off-Auto Kits?

Issue:
Need to know what the NEMA rating for the selector switch kit to be used on contactors and starters.

Product Line:
Contactors and Starters

Environment:
NEMA Contactors and Starters

Resolution:
The 9999SC8 is NEMA 1, 4 and 12/3R. The 9999SC2 is rated NEMA 1.
Was this helpful?
What can we do to improve the information ?