Technical FAQs

Ask a Question

How can Main display be changed on Process Drives to display Motor Frequency?

Issue:
How can Main display be changed on Process Drives to display Motor Frequency?

Product Line:
ATV630, ATV930, ATV660, ATV960, ATV980

Environment:
All

Cause:
NA

Resolution:
Go to Main Menu, My Preferences, Customization, and Display Screen Type. Then press 2nd tab labeled MPC. Select one or two parameters that need to be displayed on Main screen.
Was this helpful?
What can we do to improve the information ?