Technical FAQs

Ask a Question

Looking for replacement linkage for a VB valve

Issue:
What is the replacement linkage for a VB-2313-500-9-29 valve body

Product Line:
Field Devices

Environment:
Maintenance

Cause:
Replacement 

Resolution:
The  AV-601 linkage kit is used with VB-2313-500-9-29 ball valve and is :
  • Required for all heating valves with MF-5X13, MP-541X, MP-551X, MPR-561X, MPR-571X, and MPR-581X actuators
  • Recommend for cooling valves with MF-5X13, MP-541X, MP-551X, MPR-561X, MPR-571X, and MPR-581X actuators
 
Was this helpful?
What can we do to improve the information ?