Technical FAQs

Ask a Question

Can I limit the amount of Amps my Batteries supply to the inverter?

Issue:
Limiting Battery Amperage export.

Product Line:
Conext XW/SW inverters

Environment:
Battery backup XW/SW system

Cause:
Trying to set a limit on the amount of amps the battery supplies at once.

Resolution:
The XW/SW inverter does not have a setting to limit the Amps supplied by the Battery. Although Max. Charge Rate limits the Amperage for charging, it does not work both ways. The maximum amount of DC amps supplied by the battery is based on the DC breaker selected and unit being used.
Was this helpful?
What can we do to improve the information ?