Technical FAQs

Ask a Question

How can the analog input be set up on the Process drives to follow 0 to 15mA vs 0 to 20mA?

Issue:
How can the analog input be set up on the Process drives to follow 0 to 15mA vs 0 to 20mA?

Product Line:
ATV630 and ATV930

Environment:
All 

Cause:
Drive is not ramping up to speed and the system is sending a max speed signal or 15mA. 

Resolution:
Program the VFD as follows:
Main menu >
Complete settings >
Input and Outputs >
Choose third TAB marked AI/AQ 
Find the Min and max analog input and set min to 0mA and max to 15mA.
Was this helpful?
What can we do to improve the information ?