Technical FAQs

Ask a Question

What is the replacement lamp for a 9001 type K or SK illuminated operator or pilot light? 

Issue:
What is the replacement lamp for 9001KP pilot light?

Product Line: 
Push buttons and Operator Interface

Environment:
North American Products

Cause:
Would like to order the replacement lamp

Resolution:
The lamp part number is determined by the light module / voltage code used. Please use the attached to determine the voltage code you have, and the appropriate replacement lamp. 

For example a 9001KP1LRR31 uses the voltage code 1LR which is a 9001KM1LR light module. This module has a replacement lamp part number of 6508805201

 
Was this helpful?
What can we do to improve the information ?