Technical FAQs

Ask a Question

What is the 4th pole rating of a 4 pole circuit breaker

Issue
What is the 4th pole rating of a 4 pole circuit breaker. Can I have more current on the 4th pole then the rating of the breaker.
 
Product line:  
Molded case circuit breakers
 
Environment:  
Powerpact L, P, and R

 
Resolution
The 4th pole of a 4-pole circuit breaker is rated to carry the same current as the other three poles. Not any more than the rated current of the breaker.
 
Was this helpful?
What can we do to improve the information ?