Technical FAQs

Ask a Question

Are the Class 9065 Melting Alloy Overload relay DC Rated?

Issue:
Are the Class 9065 Melting Alloy Overload relay DC Rated?

Product Line:
NEMA Contactors and Starters

Environment:
North American Products

Resolution:
No. The maximum power circuit and control circuit contact rating is 600 VAC only.

 
Was this helpful?
What can we do to improve the information ?