Technical FAQs

Ask a Question

What is the End cap part number for a AF-440-7 series 1, I-line aluminum feeder duct Busway?

Issue:
What is the End cap part number for a AF-440-7 series 1, I-line aluminum feeder duct Busway?

Product Line:
I Line I Busway

Environment:
Maintenance

Cause:
Replacement 

Resolution:
The end closure has been obsolete, but may be ordered as a special with catalog number ACF27EC. The part number will need to be forced onto The Oxford Busway Plant , with list pricing provided for by SQ D Sales Office. Lead time is 40 working days. 
Was this helpful?
What can we do to improve the information ?