Technical FAQs

Ask a Question

What are the kit contents of the NQMBQ2?

Issue:
What are the kit contents of  the NQMBQ2?
 
Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards and accessories sold and supported in the USA.

Cause:
Listing of components of the NQMBQ2 kit.

Resolution:
The NQCUM2 consist of the following parts:
(1) main breaker deadfront cover
(1) main breaker mounting pan
(2) main breaker deadfront stand offs
(2)  E Screws
(6)  F screws
(2) G screws
(2) H screws
(1) mian breaker label


























 
Was this helpful?
What can we do to improve the information ?