Technical FAQs

Ask a Question

Why is the webpage not working using ATV61/71 drive?

Issue:
Why is the webpage not working using ATV61 drive?

Product Line:
Altivar 61, Altivar 71, Process Drive

Environment: 
All

Cause:
Parameter Setting

Resolution:
1.9 Communications -> Ethernet -> Services 

From the Drive Menu, scroll down to 1.9 Communications and press Enter
Scroll down to Ethernet and press Enter
Set [Services] to 3 - Webpage and Email Enabled
Was this helpful?
What can we do to improve the information ?