Technical FAQs

Ask a Question

What inside the PVxxxS can caused the external breaker to tripped?

Issue:
The inverter sometimes caused the external breaker to tripped.
 
Product Line:
PVxxxS series
 
Environment:
 
Cause:
Short inside the inverter, inrush

Resolution:
Performed Locked Out and Tagged Out (LOTO) on the inverter. Check the fuses F12, F13 and F14. If any of these fuses blown then it can caused the external breaker to trip.  Visually verify for anything that may be causing a short in the AC input side of the inverter. Call 866-519-1470 option 3 & 3 for further assistance.
 
Was this helpful?
What can we do to improve the information ?