Technical FAQs

Ask a Question

Is it mandatory that you use the EMC plate on the ATV320 drive?

Issue:
Is it mandatory that you use the EMC plate on the ATV320 drive?

Product Line:
ATV320

Environment:
All 

Cause:
Wiring practice 

Resolution:
The EMC plate is not mandatory.
It is very convenient when you use shielded cables. This is used to have a very good earth for all equipment. It provides an earth connection with the same level potential which is critical for CEM.
 
Was this helpful?
What can we do to improve the information ?