Technical FAQs

Ask a Question

SCCR Ratings for Combination Starters

Issue:
Where can I find SCCR values  for NEMA Combination Starters?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
SCCR Values are printed in the Digest as well as the 8538 Catalog.  Specific values depend on the type of disconnect and/or fusing used.  Note that non-fused disconnect units do not have a combination SCCR and will only have the default UL value.
Was this helpful?
What can we do to improve the information ?