Technical FAQs

Ask a Question

Number of Wire Terminations on 2510KO Switch

Issue:
What is the maximum number of wire terminations which can be landed on each terminal of a 2510KO switch?

Product Line:
NEMA Switches - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
One wire per terminal.  If a customer needs more wires, it is recommended to use a distribution terminal block.
Was this helpful?
What can we do to improve the information ?