Technical FAQs

Ask a Question

Mounting Lugs for NSYPLM Enclosures

Issue:
What is the part number for the mounting lugs for wall mount NSYPLM enclosures?

Product Line:
Enclosures - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
There are two options for wall mounting lugs.  Either the NSYPFXPLM for stainless steel wall fixing lugs, or the NSYPFPLMG for fiberglass polyamide can be used.
 
Was this helpful?
What can we do to improve the information ?