Technical FAQs

Ask a Question

Does Schneider offer a metal mushroom maintained operator in the 30mm line?

Issue:
Do we have a metal mushroom maintained operator in the 30mm line?

Product Line:
Type K Heavy Duty Operators

Environment:
30 mm Push Buttons

Resolution:
These operators are available in black, red, and green, as well as two sizes.
The M94 operators are 40 mm, and the M95 are 60 mm diameter heads. 
In the part numbers below the "b" indicates black, "r" red, and "g" green operator heads. 
9001KR9BM94 / 9001KR9RM94 / 9001KR9GM94
9001KR9BM95 / 9001KR9RM95 / 9001KR9GM95
Was this helpful?
What can we do to improve the information ?