Technical FAQs

Ask a Question

What is the part number for the replacement external reset mechanism for the Pump Panel 8940SSC200?

Issue:
What is the part number for the replacement external reset mechanism for the Pump Panel 8940SSC200?

Product Line:
NEMA Contactors and Starters

Environment:
North American Products

Resolution (Must confirm the series):

For Series A (OBSOLETE)
Standard Solid State O/L Relay
The complete, door mounted, external reset mechanism assembly for the standard SSOL requires the following parts:
Qty 1 - 30019-113-57 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket.

Form B12 - IEC Bi-Metal Overload Relay (using LRDxx)
The complete, door mounted, external reset mechanism assembly requires the following parts:
Qty 1 - 30019-113-xx - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket.

For Series B
Standard Solid State O/L Relay
The complete, door mounted, external reset mechanism assembly for the standard SSOL requires the following parts:
Qty 1 - 30019-113-57 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket.

Form B12 - IEC Bi-Metal Overload Relay (using LRDxx)
The complete, door mounted, external reset mechanism assembly requires the following parts:
Qty 1 - 30019-113-62 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket

 
Was this helpful?
What can we do to improve the information ?