Technical FAQs

Ask a Question

What is the part number for the plug-in on delay timer for D line contactors?

Issue:
What is the part number for the plug-in on delay timer for D line contactors?

Product Line: 
Digest 177 Section 18 : Contactors and Starters IEC

Environment:
North American Products

Cause:
Needs the part number for the plug-in on delay timer for D line contactors.

Resolution:
LA4DT0U - 0 to 2 seconds
LA4DT2U - 1.5 to 30 seconds
LA4DT4U - 25 - 500 seconds
Was this helpful?
What can we do to improve the information ?