Technical FAQs

Ask a Question

What has to happen for the Battery Monitor to log a charge cycle?

Issue:
What criteria does the Battery Monitor use to count charge/discharge cycles & sync?

Product Line:
Conext Battery Monitoring System

Environment:
Battery Monitoring System in battery backup system

Cause:
Charge/Discharge count on the Battery Monitor

Resolution:
The criteria the system uses is as follows:
 
a) Discharge  = hitting discharge floor
b) Sync = hitting 100%
c) Charge cycle = a) then b) 
Was this helpful?
What can we do to improve the information ?