Technical FAQs

Ask a Question

My inverter keeps showing W49.

Issue:
Inverter keeps showing Warning 49: Battery Overvoltage warning

Product Line:
Conext XW & SW series 

Environment:
Inverter with battery backup system 

Cause:
High Battery cutout is too close to battery voltage.

Resolution:
Make sure that the selected High battery cutout is at least 2 volts higher than the typical battery voltage (bulk, absorb, float). You can also lower your battery voltages if you have room for it.
The warning will show up when the battery voltage is 2 volts under the High battery cutout.
Was this helpful?
What can we do to improve the information ?