Technical FAQs

Ask a Question

Left Hand Mounting for 9422CMP

Issue:
Can the 9422CMP cable operated mechanisms be operated with the cable on the left?

Product Line:
Cable Operated Disconnect Mechanisms - GIC Product

Environment:
US Product

Cause:
Product Installation

Resolution:
These mechanisms are designed for the cable on the right as supplied.  They are not convertible to left side operation.  Additionally, the 9422AP handles are only designed for right hand or center channel mounting.
Was this helpful?
What can we do to improve the information ?