Technical FAQs

Ask a Question

Can you use Aluminum cables with the ATS22?

Issue:
Would ATS22 accept aluminum cables or only copper?

Product Line:
Soft Starters

Environment:
Applies to ATS22

Cause:
Would like to use aluminum cables with the ATS22

Resolution:
Yes you can use aluminum cables as long as they are nickel ends to avoid any corrision

Keywords:
ATS22, aluminum cable
Was this helpful?
What can we do to improve the information ?