Technical FAQs

Ask a Question

Video: How do you select an ERMS switch, using the Schneider Electric Product Selectors tool, for a panelboard in Q2C, Quote Fast and EQM?

Issue:
Help using the product selectors tool for Square D, Schneider Electric for an ERMS switch in a panelboard

Product Line:
panelboard

Environment:
I-line

Cause:
Product selection in Product selectors

Resolution:
1. While in the product selector tool, panelboard
2. On the general screen answer all the questions by making initial panelboard requirements selections.
3. Go to the Device menu and select Main and Feeders and select the main device. You will have to make sure to select the Micrologic trip unit as standard advanced, if not already selected.
5. After selecting the main device you must select either the Power or harmonic trip unit.
6. After making all of your selections for the main, scroll down to the device options and select it.
7. Now select the drop down menu next to maintenance switch and select locally mounted - ERMS.

The following video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?