Technical FAQs

Ask a Question

What does fault 2407 means on XC\XCNA?

Issue:
The inverter faulted on AC voltage High due to the grid input voltage was out of range
 
Product Line:
XC or XCNA
 
Environment:
 
Cause:
Grid event-possible

Resolution:
This is an Error Event and not a service event. It means that the AC votlage its outside the thershold accepted by the system, once the AC voltage is back in range then the inverter will automatically start up on its own. If it does not event when other inverter adjacent to it did, then call 866-519-1470 option 3 & 3 for further assistance.
Was this helpful?
What can we do to improve the information ?