Technical FAQs

Ask a Question

What is the difference between 9001KS*K1 and 9001KS*K2?

Issue:
What is the difference between 9001KS11K1 and 9001KS11K2?

Product Line: 
Push buttons and Operator Interface

Environment:
North American Products

Resolution:
The numbers at the end are the key codes.  On the 2 position units:
K1 - You can remove the key on the Left side only
K2-  You can remove the key on the Right side only
K3-  You can remove the key on both sides.
Was this helpful?
What can we do to improve the information ?