Technical FAQs

Ask a Question

What is the retaining bolt for the PQ3620G busplug that attaches and pulls switch into busway bussing and secures the switch into place ?

Issue:
Captive bolt in retaining bracket is stripped and needs replacement , is it an available part ? 

Product Line:
I Line II Busway switch

Environment:
Maintenance 

Cause:
Replacement

Resolution:
The brackets the bolt is captive to, are rivited to the enclosure. These brackets and bolt are not field replaceable., and a new switch would need to be ordered 
 
Was this helpful?
What can we do to improve the information ?