Technical FAQs

Ask a Question

What is the current rating for a V2 Vario switch?

Issue: 
Is the current rating for V2 Vario switch, 25A or 40A?

Product Line:
Manual Motor Control Switch

Environment:
Vario Switch

Resolution:
The V2 Vario switch is rated for 25A per UL standards and 40A per IEC standards..  
Was this helpful?
What can we do to improve the information ?