Technical FAQs

Ask a Question

Can I use anti-corrosion compound for PV terminal connections for an XCNA unit

Warning:
These instructions are intended for use by authorized service personnel who have training, knowledge, and experience in:
• Installing electrical equipment and PV power systems (up to 1000 V)
• Applying all applicable installation codes
• Analyzing and reducing the hazards involved in performing electrical work
• Selecting and using personal protective equipment
Perform LOTO to make sure all energy in the inverter is zero.  

Issue:
Use of anti-corrosion compound for XCNA bus bar connection points.

Product Line:
Conext Core XCNA units

Environment:
Applications that use XCNA

Cause:
Technicians and contractors authorized to work on unit would like to know if they can use anti-corrosion compound

Resolution:
You can use anticorrosion compound but you need to make sure you use proper torque for connections.



 
Was this helpful?
What can we do to improve the information ?