Technical FAQs

Ask a Question

What you should do if you found the filter caps are bad and its fuse blown on GT250?

Issue:
Filter caps are installed in the transformer cabinet causing it to shorten its life span.
 
Product Line:
GT250
 
Environment:
 
Cause:
Over heat
 
Resolution:
You need to call into the call center 866-519-1470 option 3 & 3 to open a new case and request the filter cap upgrade kit 0J-0197. You can download the installation procedure in solar exchange.
 
Was this helpful?
What can we do to improve the information ?