Technical FAQs

Ask a Question

Can a AL400LH7 Lug be added to a LA or LH 400A I-line breaker in a QED 2 switchboard?

Issue:
Will a QED 2 switchboard accept a LH or LH frame breaker with a lug rated for 1 - 750KCMIL wire range?

Product Line:
Switchboard breakers

Environment:
QED 2 and LA/LH breaker

Cause:
Alternative lug wire range

Resolution:
Yes, the AL400LH7 Lug,  which allows up to 1 - 750KCMIL max, can be used on the LA or LH I-line constructed breaker for use in a QED 2 Switchboard.
This lug can be added in the field or at the time of selection and configuration of the switchboard,  in product selectors, under special pricing, using the Rapid TAG sheet that is available to Schneider Electric Sales personnel. This option would require contacting a local distributor who will work with the local Schneider sales office.
Was this helpful?
What can we do to improve the information ?