Technical FAQs

Ask a Question

What is the part number for the door kit for a Homeline CHOM60120M Load Center?

Issue :
Load center accessory

Product Line :
Canadian Homeline Load centers

Environment:
Door Kit 

Cause:
Application 

Resolution:
The door kit part number is CHOMDK602 and this door kit comes standard with a lock kit (PK3FL) from the factory, so NO additional lock kit is needed.

Was this helpful?
What can we do to improve the information ?