Technical FAQs

Ask a Question

What is the packing gland nut for obsoleted TAC VB-9XXX Globe Valves

Issue:
What is the packing gland nut for obsoleted TAC VB-9XXX Globe Valves ?

Product Line:
Valves and Actuators 

Environment:
Maintenance

Cause:
Replacement 

Resolution:
These parts are no longer offered for sale. Recommendation is to replace the VB-9000 valve body, 1-1/2" and 2", with VB-7000 Valves + replace actuator and linkage.
Replace Cartridge for 1/2" - 1-1/4"  VB-9000's with YBA-622
2-1/2" - 6" Replacement Cartridge is YBA-652-2
Was this helpful?
What can we do to improve the information ?