Technical FAQs

Ask a Question

Can I use my XW AC2 terminals as my Grid terminals?

Issue:
I have a damaged terminal on AC1 Grid of the XW6048. Is it possible to bring Grid power through the AC2 Gen terminals. The XW6048 is only being used to charge batteries.

Product Line:
Conext XW series

Environment:
XW system with Grid used to charge the batteries only

Cause:
Damaged AC1 terminals, and grid only used to charge batteries

Resolution:
Since Grid is being used ONLY to charge your batteries you will be able to use the AC2 terminals. Remember to adjust your settings to Gen Support (AC2) and not Grid Support settings. Again sell mode would be disabled, and AC2 would be your main source that will be used to charge your batteries.
Was this helpful?
What can we do to improve the information ?