Technical FAQs

Ask a Question

Do Altivar Drives have UL other than UL508C?

 Issue:
Do Altivar Drives have UL other than UL508C?

Product Line:
Altivar AC Drive

 
Environment: 
All

 
Cause: 
AC Drive ratings

 
Resolution:
Per Jim Crook, Product Line Engineering, any certifications required for an application, that are not supplied based on Schneider Electric testing are the responsibility
of the OEM or Engineer that specifies the equipment.  UL508C is specifically for Power Conversion Equipment.
Was this helpful?
What can we do to improve the information ?