Technical FAQs

Ask a Question

Can Model 6 MCC (Motor Control Center) be ordered , bought , with reduced height enclosure from the standard 90"H enclosure with 72" of bucket mounting space?

Issue:
Space limitations for MCC needed for Nema 1 construction. N3R construction cannot have reduced height feature. 
 
Product Line:
Model 6 MCC 

Environment:
Application

Cause:
Space restriction 

Resolution:
Nema 1, 1A  gasketed constructed enclosures can be made with 12",18", and 24" reduced height enclosures .

12" reduction would create a 78"H enclosure with 60" of bucket space
18" reduction would create a 72"H enclosure with 54" of bucket space 
24" reduction would create a 66"H enclosure with 48" of bucket space.

Only 18" H reduction can be quoted thru a SQ D/SE Distributor and Product selectors.
12" and 24" reductions would need to go thru a Local SQ D/SE Sales Office Sales Rep. 
Was this helpful?
What can we do to improve the information ?