Technical FAQs

Ask a Question

What is the replacement door reset assembly for 8606SFA1?

Issue:
What is the replacement door reset assembly for 8606SFA1?

Product Line:
Reduce Voltage Starters

Environment:
North American Products

Resolution
The complete, door mounted, external reset mechanism assembly requires the following parts:
Melting Alloy (Overloads using Type CC Thermal Units)
Qty 1 - 30019-113-90 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700  - Gasket (required on NEMA Type 12 enclosures).
Was this helpful?
What can we do to improve the information ?