Technical FAQs

Ask a Question

Converting Coil 31041-402-02 from 240V to 120V

Issue:
How do you convert coil part number 31041-402-02 from 240V to 120V?

Product Line:
NEMA Starters and Contactors - GIC Product

Environment:
US Product

Cause:
Product Application

Resolution:
Remove all power to the device and the control circuit before making changes.  The coil should have a jumper between terminals 2 and 3, and the control wiring should be landed on terminals 1 and 4 for 240V operation.  For 120V operation, the control wiring should remain in place, but the jumpers need to be changed.  Remove the jumper between terminals 2 and 3.  Add two jumpers, one between terminals 1 and 2, and one between terminals 3 and 4.  This shown in the attached diagram.
 
Was this helpful?
What can we do to improve the information ?