Technical FAQs

Ask a Question

Coil Consumption for 8903PB Coils

Issue:
What is the coil consumption for the 9998PBV coils?
9998PBV02
​9998PBV08
​9998PBV39
​9998PBV28

Product Line:
NEMA Panel Board Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
9998PBV02 - 120V coil, 1800VA
​9998PBV08 - 208V coil, 2496VA
​9998PBV39 - 240V/277V coil, 2770VA
​9998PBV28 - 480V coil, 2400VA
Was this helpful?
What can we do to improve the information ?