Technical FAQs

Ask a Question

8501R Transition From Series C to Series D

Issue:
What change was made from series C to series D on the 8501R type relays?

Product Line:
NEMA Control Relays - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
Series C was eliminated in 2014 and replaced with series D.  The series change was to signify a change in the cover to the device.  There is no functional or compatibility issue associated with this change.
Was this helpful?
What can we do to improve the information ?