Technical FAQs

Ask a Question

Does Schneider offer DC rated NEMA contactors and starters?

Issue:
Do Square D still offer DC rated power ples or DC coils for our NEMA contactors?

Product Line:
NEMA Contactors and Starters.

Environment:
8502, 8536, 8702 and 8736

Cause: 
Product Selection 

Resolution:
No, DC rated power poles or DC control coils for NEMA contactors and starters are no longer offered.
These starters were divested in 2003, customers should contact EC&M (The Electric Controller and Manufacturing Company) at 1-800-240-1230 (toll free) for more information on NEMA style DC devices. 
Was this helpful?
What can we do to improve the information ?