Technical FAQs

Ask a Question

Video: Removing Lugs from 400/600A Unit Mount PowerPact Breakers

Issue:
How to take out a lug in a Unit-mount PowerPact 400a or 600A breaker

Product Line:
Circuit Breakers

Environment:
Applies to Unit-mount version of the PowerPact 400A and 600A breaker

Resolution:
To remove the lugs, first de-energize the breaker and the gear.
-Remove the lug cover
-Remove the lower wire binding screw closest to the breaker frame

-Remove the lug mounting screw
-Pull the lug out of the breaker.

See the video as reference:

Was this helpful?
What can we do to improve the information ?