Technical FAQs

Ask a Question

What are the contact arrangement for Hermetically sealed contact blocks for 30 mm operators?

Issue:
What are the contact arrangement for Hermetically sealed contact blocks?

Product Line:
9001 Type K, SK and KX Electrical Components

Environment:
30mm Push Buttons

Resolution:
There are two types of hermetically sealed contact blocks, the 9001KA4# and the 9001KA5#. The 9001KA4 line is suitable for use on low energy level circuits. 

9001KA41 / 9001KA51 - 1 normally open, 1 normally close
9001KA42 / 9001KA52 - 1 normally open
9001KA43 / 9001KA53 - 1 normally close
9001KA44 / 9001KA54 - 2 normally close
9001KA45 / 9001KA55 - 2 normally open
Was this helpful?
What can we do to improve the information ?