Technical FAQs

Ask a Question

What is the maximum current that can be delivered from the internal 24 volt power supply on Lexium 28?

The internal 24 volt power supply can provide a maximum of 200ma at 24vdc (available at pin 17 of the 50 pin signal connector CN1)
This 24 volt source is provided as a means to supply I/O switches and or proximity switches that are connected to the inputs of LXM28


Rev 8-1-18
 
Was this helpful?
What can we do to improve the information ?