Technical FAQs

Ask a Question

Is there a pressure switch that turns on at a given pressure, but stays on until there is no pressure.

Issue:
Would like to select a pressure switch that will turn on at # psi and stay on until 0 psi 

Product Line:
Pressure Switches - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
We do not offer a pressure switch that will turn on at a certain pressure and then stay on until there is no pressure in the system 
Was this helpful?
What can we do to improve the information ?