Browse FAQs

What is the acceptable signal voltage input range for DIG encoder module VW3M3402 ?

Published date: 04 September 2019

The optional DIG encoder module, VW3M3402, is designed to accept 5 volt signal levels only.
Damage will occur to the encoder module if signals higher than 5 volt are applied to the inputs.
Therefore it is not permissable to use encoders that have 24 volt logic ouputs.

VW3M3402 is designed for 5 volt TTL

Rev 9-4-19


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.