Technical FAQs

Ask a Question

Does Schneider Electric offer motor type BRX184 found on a W&H printing press?

The BRX184 motor type is a special customized product for the company W&H  (Windmoeller & Hoelscher)
Because this is a customized product it is not available for purchase directly from Schneider Electric.
The OEM machine builder, W&H, has a contract with our manufacturing facility in Germany that this motor is only available to W&H.
Customers must contact W&H with their support questions or for spare motors of this type.

.
Rev 8-8-17
Was this helpful?
What can we do to improve the information ?