Technical FAQs

Ask a Question

What are the part numbers for the encoder cables used with BMH or BSH servo motors

The encoder cables listed in the attached file are compatible with all BMH or BSH motors when used with Lexium 32 drives.
Choose based on the required length.

Rev 7-23-18
Was this helpful?
What can we do to improve the information ?